Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Product List
LPC29xx Microcontrollers Slide 54
Each timer consists of a prescale counter (PR register) and a timer counter (TC register). The prescale counter is incremented at every cycle of the system clock. As soon as the prescale counter matches the prescale value contained in the value register it is reset to 0 and the timer counter is incremented. The timer block contains four capture circuits. The capture functionality allows measuring the time of an external event. Depending on configuration, a rising or a falling edge of the input can cause a capture event. The timer block contains four match circuits, each of which can be programmed with an individual match value and a specific action-on-match. Once the counter value matches one of the programmed match values in the MR register, one or more of the following actions can occur: a reset in the counter and prescaler, stopping of the counter, generation of an interrupt, or generation of an external notification. If interrupts are enabled and an interrupt condition occurs (match value reached or capture event received) the timer generates an interrupt.
PTM Veröffentlicht am: