Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
hi speed timer
The high speed timer, millisecond timer, and the watchdog timer are inherent to the LPC3000 family. The four general purpose timers are adopted from the LPC2000 family and explained in the next slide. Some key points from the first block - the high speed timer is clocked by the peripheral clock, the millisecond timer is clocked by the 32 KHz RTC clock, and the watchdog can be used as a standard timer if not used as a watchdog.
PTM Veröffentlicht am: