Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
3250 block dia
The heart of the LPC3250 is the ARM9ESJ-S core integrated with 32KBytes of instruction and data cache. The CPU subsystem also comprises of the vector floating point coprocessor (VFP9), which is critical for DSP based applications. This core also supports embedded trace. Except for the LPC3220, all other devices in this series are provided with 256KBytes of on-chip SRAM. The external memory interface incorporates a NAND flash controller and SDRAM controller together with an interface for an SD card. Highlighted are three key peripherals: the Ethernet controller, the USB block which can be configured as a full speed device, host, or OTG, and the LCD controller. Connecting all the modules together is the multi-layer AHB matrix.
PTM Veröffentlicht am: