Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
rtc block
The RTC block in the LPC3250 has an ultra low power design and is ideal for battery powered systems. It has a dedicated 32 KHz oscillator, 128 Bytes of very low voltage static RAM, and interrupt mechanisms using match registers to come out of STOP mode. Also, a point to note is that the RTC power domain is isolated from the rest of the chip. An output pin is also included to assist in waking the chip when it has power removed to all functions except the RTC and Battery RAM.
PTM Veröffentlicht am: