Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 2
The ARM7TDMI-S core, a commonly implemented ARM7 core, has a 3 stage pipeline and uses a Von Neumann Architecture.  The resulting core generally achieves about 1.9 clock cycles per instructions on average. The “TDMI-S” part of the core name specifies more about the core and its features.  The T indicates that the Thumb instruction set is supported, the D indicates that there are debug features available on the core, and the M indicates support for 64-bit results with an enhanced multiplier.  Additionally, the I indicates that there are EmbeddedICE logic extensions provided to support advanced debugging capabilities and the S indicates the fully synthesizable nature of the intellectual property (IP) for the ARM7 core.
PTM Veröffentlicht am: