Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 3
The ARM7 RISC architecture uses “pipelining” to increase its performance – something that is rarely seen in the old CISC platforms. The program counter points to the instruction being fetched – which can be a problem if an unanticipated instruction is executed. However, during normal operation, while one instruction is being executed, its successor is being decoded and set up for execution while a third instruction is being fetched from memory.
PTM Veröffentlicht am: