Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 4
There are two modes that the ARM7 core can run in – ARM and Thumb.  ARM is the native 32-bit mode for the ARM7 core.  The Thumb mode, on the other hand, is a mode in which each instruction is 16-bits – this can decrease code size, but will result in slower overall execution since all instructions will be decompressed to a native ARM instruction during decode.  The above slide compares the program counter (PC) indexes as these two modes proceed through the 3-stage instruction pipeline.
PTM Veröffentlicht am: