Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Cooling Fan Motor Drivers Slide 21

Shown on this slide, the LV8068V is a single phase bridged transformerless fan motor driver that can combine the drive signal with PWM to deliver a highly efficient and silent motor drive. It has a high maximum VCC of 18 V giving it a large safety margin when running from a 12 V source.

PTM Veröffentlicht am: