Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Cooling Fan Motor Drivers Slide 25

The LB11685AV is a 12 V system, 3-phase, sensor-less fan motor driver. Maximum VCC is 19 V, providing a good safety margin in 12 V systems. It is controlled by pulse amplitude modulation and has many safety features like current limiting and thermal shutdown. For the latest list of fan motor drivers, be sure to check the web at www.onsemi.com. Design resources such as the availability of demo boards, packaging, and application notes can also be found there to aid in a design.

PTM Veröffentlicht am: