Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Cooling Fan Motor Drivers Slide 5

On this slide the driving waveforms for a BTL output and a PWM switched output are shown side by side. Notice how smooth the output current is for the BTL drive on the left. The slow rise and fall of the output voltage leaves the transistors in their linear region and results in more power usage in the driver. The LV8068V used for the BTL drive is also capable of PWM driving via an external input pin. On the right can be seen PWM driven waveforms. Notice in the lower right the quick switching of the output transistors. This causes less power to be dissipated in them and results in lower power consumption. The disadvantage is the more noisy output current waveform seen in the lower right Iout waveform.

PTM Veröffentlicht am: