Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Accessories

The V8 Adaptor (pictured here on the left) offers a quick cabling solution that lets users wire up eight separate relays at once, drastically reducing wiring time. The Partition Plate (upper middle) allows users to separate their relays on the rail. Notice that the shape is similar to the PLC Relays and that there are removal “windows” on the sides, this allows users to use the continuous blade bridges to bridge straight through the partition plate. The Fuse Adaptor (pictured on the right here) allows users to integrate a fuse into the relay module. Simply plug the fuse adaptor in where the relay would plug in, and then put the relay in the socket of the adaptor and there will now be an extra layer of protection, provided by the fuse.

PTM Veröffentlicht am: