Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of ROHM 4th Generation SiC MOSFETs - Flexible On-State Gate Voltages

ROHM’s 4th Generation MOSFETs not only offer efficient performance but they are also easier to drive. The recommended turn-on gate voltage is flexible between 15 V and 18 V, making it compatible with other power devices such as silicon IGBTs. When 15 V gate bias is used for the conduction state instead of 18 V, the MOSFET shows a small increase in ON-resistance by 7%. This is much more manageable than the 30% difference in ON-resistance for the previous Generation device. In a converter-level test, it is confirmed that driving the 4th Generation SiC MOSFET at 15 V gate bias does not significantly impact its overall power conversion efficiency, although 18 V gate voltage still has an advantage to reduce the conduction losses to a very minimum.

PTM Veröffentlicht am: