Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of ROHM 4th Generation SiC MOSFETs - Conduction Loss

In this application example, a buck converter is tested for power conversion efficiency using both 3rd and 4th Generation SiC MOSFET devices with a similar chip size. Because of its much lower ON-state resistance, the 4th Generation MOSFET performs significantly better in the entire range of output power. The thermal images compare the two SiC MOSFETs operating at 5 kW output power level, demonstrating substantially less heat generation in the newer MOSFET due to its conduction loss improvement.

PTM Veröffentlicht am: