Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
CMOS-Slide11

This last example is using an OpAmp in the Main Inverter of an automotive system to detect current. On the right is the motor and on the left is the MCU. Inserting an OpAmp in between allows the designer to amplify the voltage, allowing the MCU to properly detect the motor status.

PTM Veröffentlicht am: