Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
mediagauge-slide14

In the graph shown here, you can see how the user can program the high and low set points to control when the relay would turn on and off. Input pressure values below the low limit set point or higher than the high limit set point will result in a limit switch output of 0 Vdc. Input pressure values within the control set point limits (between the low and high set points values) will result in a limit switch output that follows the external power source.

PTM Veröffentlicht am: