Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
mediagauge-slide9

The peak hold function captures high pressure spike values and stores them in memory. The zero adjustment function allows the display to be zeroed out for maximum accuracy of measurements or allows the operator to reference the gauge to the input port. The MG-MD model has programmable high and low pressure set points for use with the 4-20 mA output and switch.

PTM Veröffentlicht am: