Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
mediagauge-slide8

MediaGauge™ digital pressure gauges offer standard features, which includes an easy to read four digit display. The sensor is housed in a rugged NEMA 4X housing. The digital gauges feature a battery saver mode which automatically shuts the MediaGauge off to conserve the battery life. Only one gauge is needed to measure pressure in different units of measure with the MediaGauge displaying the pressure value in either PSI, BAR or MPA.

PTM Veröffentlicht am: