Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
fp-sns-allmems1 hw addl
This slide contains additional information for the hardware development platform. If the target STM32 Nucleo development board is the Nucleo-L476RG, the user needs to close the soldered bridges named SB12, 16, and 17. Regardless of which STM32 Nucleo board the user selects for his/her development, the three ZERO-ohm resistors SB25, SB26, and SB27 need to be removed from the X-NUCLEO-IKS01A1 MEMS sensors expansion board.
PTM Veröffentlicht am: