Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
sw install STM32 ODE function packs STMicro site Google Play STBlueMS
Shown here is the step by step software installation procedure. Go online to ST.com and insert in the search engine the keyword “FP-SNS-ALLMEMS1”. A zip file will be downloaded; unpack it. Next, select the target hardware platform by browsing the folder tree starting from the “Projects” section. The reference application code will support multiple Integrated Development Environments (IDEs). The user will choose the one that matches his/her needs. At this point, the user will compile and flash the code on the selected target hardware platform. The last step is to download and run the ST BlueMS application on the user’s smartphone. Note that this step by step software installation procedure is common to all the Function Packs available on ST.com (and it is not specific only to FPs discussed in this presentation).
PTM Veröffentlicht am: