Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
bluems app sdk Android github iOS github
The companion application for the smartphone is named “ST BlueMS”. This is the keyword that the user should search for while browsing either Google Play or the App Store. Besides the app being available in these stores, a Software Development Kit suitable for both Android and iOS devices is available from the GitHub links shown here. On the two GitHub repositories, the user can find the source code that corresponds to the ST BlueMS application.
PTM Veröffentlicht am: