Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 20

Looking at some of the details behind this platform, it can be seen that this is USB-IF certified. Beyond that, TI has certification for five device specializations: blood glucose meters, blood pressure monitors, digital thermometers, pulse oximeters, and weight scales. Also featured are code-efficient stacks that take a minimal amount of memory, and documentation to support integration of these stacks in the customer’s solutions. Ideally, the developer would take the stacks that are offered, and using the sample application layer develop a full-blown application applying their expertise. There are two options offered; the USB PHDC protocol layer, and the full Continua-certified solutions, including the PHDC along with the IEEE 11073 layers. For additional information the customer can visit the website at www.ti.com/usbplatform. If needed, customers can send an email to medical_usb@ti.com.

PTM Veröffentlicht am: