Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 29

In this slide the finger probe with the two LEDs is shown, and the detector (photo diode) of the light that has not been absorbed by the finger, which feeds into the MSP430. Also, a self-contained system can be seen that is performing signal conditioning with the A/D converter, the op-amps, as well as the DAC, and providing some control to the LEDs. An integrated LCD driver is used to display the blood oxygenation or the heart rate of the patient. All of this powered by a coin cell.

PTM Veröffentlicht am: