Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 34

In summary, as portability becomes a growing trend in medical products, manufacturers are seeking technologies that reduce the design complexity and time in developing the finished product. In most of these medical equipment solutions, the actual physiological signals are analog and require signal conditioning techniques, such as amplification and filtering, before they can be measured, monitored, or displayed. The MSP430 microcontroller MCU offers a platform of ultra-low-power processors with the high integration of the complete signal chain that is required for applications such as personal blood pressure monitors, spirometers, pulse oximeters, and heart rate monitors.

PTM Veröffentlicht am: