Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
LM5017 Synchronous Buck Converter and COT Slide 14
One fairly simple way to reduce the output ripple is to add a capacitor across the upper feedback resistor. As shown in the diagram on this slide, by adding that capacitor an AC coupling path is set up so the ripple voltage at the feedback pin is essentially the same as the ripple voltage at the output. Therefore the output voltage ripple is reduced.
PTM Veröffentlicht am: