Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
LM5017 Synchronous Buck Converter and COT Slide 18
Shown on this slide is a summary of the various ripple configurations. What is referred to as type one, on the left, is the most simple. The type two in the center is essentially the same, but features the coupling capacitor that was discussed. The last is the ripple generation network, shown on the right as type three. Shown on the lower left is a reference to an application note, AN-1481 which is a resource for additional information.
PTM Veröffentlicht am: