Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Surface Mount Coupled Inductors Slide 12

Another benefit when using a dual inductor in a SEPIC or Zeta Converter is that the inductance can be 50% less because the ripple current will split between the two windings. This will reduce the DC resistance and improve the overall efficiency. In the table we show a dual inductor vs. two similar single inductor models. The DC resistance is between 36-44% less when compared to the single winding inductors.

PTM Veröffentlicht am: