Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Surface Mount Coupled Inductors Slide 15

In summary, the HM78D-1210 coupled inductors are extremely versatile in that they can be utilized as a power inductor, a dual inductor, a 1:1 turns ratio transformer or as an autotransformer. One of the most common applications is a high current power inductor in a buck or boost converter. Another application is a (SEPIC) using a boost controller, a ZETA converter using a buck controller or a dual voltage output buck converter. Other applications include a coupled inductor in a two-port filter and as an autotransformer where isolation is not required.

PTM Veröffentlicht am: