Basics of USB

Choosing the correct USB can be a difficult task, especially for someone who is unfamiliar with all the different types. An article I recently wrote lays out the background of USBs and the different options, along with a visual providing what the male and female version of each looks like. Some of the more widely used types are called out below to help ease the selection process.


  • Type A
    • Flash Drive
    • Power Cables

  • Type Micro B
    • Cell phone charging

  • Type C
    • Newly adopted as cell phone charging connectors
    • Only current reversible option

There are many other types covered in the article, along with the different speeds each type is capable of supporting, a bit of history on the connector, and links to the product on DigiKey’s website. Shown in the image is a Type A Male to Type Micro B Male cable assembly.

Informazioni su questo autore

Image of Ashley Awalt

Ashley Awalt, Applications Engineering Technician, lavora in DigiKey dal 2011. Ha conseguito una laurea tecnico-scientifica in Electronics Technology & Automated Systems presso Northland Community & Technical College attraverso il programma di borse di studio DigiKey. Nel suo ruolo attuale assiste nella creazione di progetti tecnici unici, documentando il processo e partecipando alla produzione di video multimediali dei progetti. Nel tempo libero, ad Ashley piace - ohhh, cos'è il tempo libero per una mamma?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum