mu;
7
G6J-Y Surface-mounting Relay
■Approved Standards
UL/C-UL Recognized. (File No.E41515)
■Precautions
●Please refer to “PCB Relays Common Precautions” for correct use.
●Long Term Current Carrying
Under a long-term current carrying without switching, the
insulation resistance of the coil goes down gradually due to the
heat generated by the coil itself. Furthermore, the contact
resistance of the Relay will gradually become unstable due to the
generation of film on the contact surfaces. A Latching Relay can
be used to prevent these problems. When using a single-side
stable relay, the design of the fail-safe circuit provides protection
against contact failure and open coils.
●Handling of Surface-mounting Relays
• Use the Relay as soon as possible after opening the
moistureproof package. (As a guideline, use the Relay within
one week at 30°C or less and 60% RH or less.) If the Relay is
left for a long time after opening the moisture-proof package,
the appearance may suffer and seal failure may occur after the
solder mounting process. To store the Relay after opening the
moisture-proof package, place it into the original package and
sealed the package with adhesive tape.
• When washing the product after soldering the Relay to a PCB,
use a water-based solvent or alcohol-based solvent, and keep
the solvent temperature to less than 40°C. Do not put the relay
in a cold cleaning bath immediately after soldering.
●Claw Securing Force During Automatic Insertion
During automatic insertion of Relays, make sure to set the
securing force of the claws to the following values so that the
Relay characteristics will be maintained.
●Environmental Conditions During Operation, Storage,
and Transportation
Protect the Relays from direct sunlight and keep the Relays
under normal temperature, humidity, and pressure.
●Mounting Latching Relays
Make sure that the vibration or shock that is generated from
other devices, such as Relays in operation, on the same panel
and imposed on the Latching Relays does not exceed the rated
value, otherwise the Latching Relays that have been set may be
reset or vice versa. The Latching Relays are reset before
shipping. If excessive vibration or shock is imposed, however,
the Latching Relays may be set accidentally. Be sure to apply a
reset signal before use.
●Maximum Allowable Voltage
• The maximum voltage of the coil can be obtained from the coil
temperature increase and the heat-resisting temperature of
coil insulating sheath material. (Exceeding the heat-resisting
temperature may result in burning or short-circuiting.) The
maximum voltage also involves important restrictions which
include the following:
• Must not cause thermal changes or deterioration of the
insulating material.
• Must not cause damage to other control devices.
• Must not cause any harmful effect on people.
• Must not cause fire.
Therefore, be sure not to exceed the maximum voltage
specified in the catalog.
• As a rule, the rated voltage must be applied to the coil. A
voltage exceeding the rated value, however, can be applied to
the coil provided that the voltage is less than the maximum
voltage. It must be noted that continuous voltage application to
the coil will cause a coil temperature increase thus affecting
characteristics such as electrical life and resulting in the
deterioration of coil insulation.
●Coating
Relays mounted on PCBs may be coated or washed. Do not
apply silicone coating or detergent containing silicone, otherwise
the silicone coating or detergent may remain on the surface of
the Relays.
●Other Handling
Please don’t use the relay if it suffered the dropping shock.
Because there is a possibility of something damage for initial
performance.
Contact form Coil rating Contact rating Number of test
operations
DPDT (2c) G6J-2P-Y, 2FS-Y, 2FL-Y: 3 to 24 VDC
G6JU-2P-Y, 2FS-Y, 2FL-Y: 3 to 24 VDC
1 A, 30 VDC at 40°C
0.5 A, 60 VDC at 40°C
0.3 A, 125 VAC at 40°C
6,000
Correct Use
Direction A: 4.90 N max.
Direction B: 9.80 N max.
Direction C: 9.80 N max.
Secure the claws to the area indicated by shading.