Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide12

Most of the time, instrumentation amplifiers cannot tolerate input voltages beyond their supplies. Most instrumentation amplifiers contain ESD diodes at the supply inputs. If a voltage goes beyond the supplies, one of these ESD diodes can turn on. If the current is not limited, the part will be damaged by the excessive current flow. The In Amp is typically the first IC in the signal chain, connected to the outside world through leads. Accidents can happen – for example being connected to the wrong sensor, or even the right sensor when the In Amp’s power is off. In Amp circuits be designed to handle these fault conditions.

PTM Veröffentlicht am: