Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide14

Another option is to use protection resistors before the instrumentation amplifier. These protection resistors limit the current going into the ESD diode so the part is not damaged. Normally the amount of current the instrumentation amplifier can handle flowing into its inputs is specified in the datasheet. If no value is specified, a maximum current of 5mA can typically be assumed. Choosing the value of the protection resistors is a tradeoff – larger value resistors provide more protection but contribute noise and may convert input offset currents into an offset voltage error. The resistors used for protection can be the same ones used for RFI (radio frequency interference) protection.

PTM Veröffentlicht am: