Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide7

An example is probably the best way to illustrate this. The AD8231 is shown, which uses internal op amps that have rail to rail inputs and rail to rail outputs. n this example, the AD8231 is configured with a gain of four and driven with a 1V differential voltage. This 1V differential input multiplied by a gain of four should result in 4V at the output. In order to illustrate the effect of common mode voltage near the rails, this example has used a common mode voltage of 4V. This results in a positive input voltage of 4.5V – pretty near the rail. However, the inputs and outputs are still well within the range of the AD8231’s internal rail to rail op amps.

PTM Veröffentlicht am: