Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide13

One solution is to use components that are specifically designed for overvoltage conditions. Some parts include voltage protection that allow voltage beyond the supply rails. Their datasheets typically advertise this feature and their absolute maximum ratings will show voltages beyond the supplies are allowed. The input stage for the AD8226 and AD8227 is shown here.

PTM Veröffentlicht am: