Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 2

A single CMOS switch or a single channel of a CMOS multiplexer essentially consists of an N-channel and a P-channel MOSFET transistor in parallel as outlined in the diagram. The respective drains and sources of the two transistors are tied together to become the switch terminals, while the gates of the two transistors are driven to control the on/off action of the switch. Essentially, the N-channel is on for positive gate-to-source voltages and off for negative gate-to-source voltages, while the P-channel does just the opposite.

PTM Veröffentlicht am: