Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 3

One of the benefits of having NMOS and PMOS in parallel with one another is a wide input voltage range from Vdd to Vss. The switch is fully bi-directional which means that the input signal can go from Source to Drain or vice versa. The parallel combination of NMOS and PMOS also gives a relatively constant RON over the input signal range.

PTM Veröffentlicht am: