Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 8

When the switch is off, leakage current can introduce errors as shown in this slide. The leakage current flowing through the load resistance develops a corresponding voltage error at the output. The iCMOS process and the ADG12xx parts offer excellent linear leakage performance up to 80°C.  Leakage variation with temperature is an important consideration for many customers.

PTM Veröffentlicht am: