Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 4

One of the main limitations of the parallel structure of an NMOS and PMOS switch is the increased capacitance between the signal lines and GND as well as between the source and the drain. These capacitances affect the frequency response of the switch in both on and off cases and directly impacts the switch bandwidth and off isolation performance. The advantage of the NMOS is that it reduces the capacitances mentioned above and provides a better frequency response compared with the parallel CMOS structure. Because of these advantages, the NMOS switch is recommended for high speed applications with high data rate links (USB, Ethernet, SONET) and wide band analog applications (HDTV).

PTM Veröffentlicht am: