Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
RFID-Slide11
Microchip is also active in the automotive industry, using the same LF technology combined with UHF uni- or bidirectional technology. Applications include immobilization systems, passive entry go. Manufacturing and logistics (both in the automotive and in the industrial/consumer industry) is another application field. Tags that contain production information increase the uptime of production lines. In that sense, the tags act as a backup of the production control units. The final application group to be mentioned is the broad field of brand protection and product authentication applications.
PTM Veröffentlicht am: