Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
RFID-Slide23
Another important tool is the new ATA5505 kit. The ATA5505 is an 8-bit AVR microcontroller with an LF RFID reader peripheral. In fact, it is a complete reader in a single package. The AVR MCU provides 16kB of Flash, which is sufficient for the RFID code and additional user code. The kit communicates with the same GUIs as previously explained via a USB interface. As with all Microchip RFID kits, several tags are included for immediate use and testing.
PTM Veröffentlicht am: