Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
RFID-Slide14
The ATA5575 is the latest generation of Microchip's IDIC® chips (IDentification IC). It is based on the design of the successful ATA5577 with the same high level of performance. The portfolio is composed of two different versions, addressing the two main LF RFID markets. The ATA5575M1 targets access control applications with a dedicated unique format. In the past, factory-preprogrammed R/O tags have been used for that purpose. New market trends require more flexibility in the way this number is composed, and a faster time to market. These requirements are perfectly met by the ATA5575M1. The ATA5575M2 is designed for animal identification (FDX-B and FDY-A modulation according to ISO 11784 and 11785). It also covers FSK access control applications.
PTM Veröffentlicht am: