Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
CliQ Series DIN Rail Power Supplies Slide 21

The CliQ M series is designed with the latest feature in the CliQ family of products: the Advanced Power Boost (aka APB). The APB feature is useful when multiple loads are connected in a system and a large outrush current could be drawn due to one fault load. This will be detected by APB. The APB feature will trip the circuit breaker on the current path of the fault load due to high current. This prevents the system from shutting down while the other connected current paths continue to operate without interruption.

PTM Veröffentlicht am: