Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Example Resources: App Notes and MIPI Utility 1

Shown here is an example of the documents section. The user manuals, data sheets, and application notes are all here. Efinix has several application notes on the MIPI demos, including a spreadsheet utility to help the customer configure the MIPI interface. These documents are important to read if the customer is planning on using the MIPI/CSI hard blocks. All this data is open to any user to see, as there is no password required. Access to this information is available under the support button in the upper right on Efinix Inc Web page, navigate there and then hit documentation.

PTM Veröffentlicht am: