Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Camera Application Examples – MIPI/CSI

This slide and the next one will show some examples that are more camera specific. This slide shows application examples that are more MIPI/CSI oriented. The examples are with either one, two or three MIPI/CSI camera interfaces and outputs that can be MIPI/CSI or other interfaces. Simple bridging of the CSI to some other standard can be accomplished or multiple cameras with various levels of Image processing, depending on the size of the Trion® device that is chosen. The processor interconnects are MIPI/CSI, parallel, PCIe, USB, and a variety of specialized interconnects. The value of having an FPGA, is that Efinix can interface to any other device very easily. One such example is that Efinix can interface to a standard device like a USB controller and do some preprocessing in the FPGA and the rest of processing, if any, are done by the processor that has USB interconnect needed. With the hardened DDR DRAM controller, a frame buffer can also be created for temporary storage. These are the perfect devices for Edge analytics, as there are many choices of devices to perfectly match the power/and system cost requirements. Migration within a package is supported, so any of the devices in the same package allow the customer to choose what size device is needed after the final debug.

PTM Veröffentlicht am: