Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Camera Application Examples – Non-MIPI/CSI

In this second camera application, Efinix is showing non-MIPI/CSI examples. The upper examples here are somewhat of SOC examples, where not only is a camera input being interfaced, but display and various other peripherals are being handled within the Trion® devices. In addition to the bridge functions, the display control and image processing is also handled by the Trion device. On the bottom of the slide is an example of interfacing a camera sensor to a USB device which is a common application. In this case, Efinix is interfacing to 7:1 LVDS on the camera side, which is another common camera interface standard that some may refer to as camera link. Conversion to USB could be needed as part of any overall solution and could be added to many of the examples shown previously.

PTM Veröffentlicht am: