Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Summary

In summary, Efinix provides low cost Evaluation kits that can help the customer understand the features of the Trion® devices. Efinix’s T8 and T20 Development kits allow the customer to prove out the concept of a design and interconnect with their board or other development boards, prior to spinning a new board of their own. The T20 MIPI/CSI kit interconnects to some standard cameras and spinning a daughter card is simple and easy, which will allow the customer to do some interoperation with a camera sensor of choice. The Efinity tools work elegantly on Red Hat, CentOS, and additionally on Windows. The customer can choose to use the Efinity Graphical UI or run the tools from scripts. The tool and boards are all very low cost and Efinity is a full featured, fully integrated Verilog/VHDL to bit Generation Development Tool. With the small packages, low power, and volume optimized price the customer can accomplish much of the edge intelligence, IoT, processing, control and vision application with the whole family of Trion devices from Efinix Inc. Lastly Efinix has many use cases of customers developing their products using the Trion devices to create differentiation that enable their own customer successes.

PTM Veröffentlicht am: