Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List Associated Content
Image of Efinix Trion® FPGA and How They Work - Slide12

Each FPGA has a number of phase locked loops, or PLLs, for use in a design. The PLLs are a way to create alternate clock frequencies based on input frequencies. The frequencies are defined by the setting of N, M, O, and C parameters as shown here. The customer can also use the PLL to synchronize clocks and to also generate clocks with different phase relationships. The Efinity® tool has a PLL wizard to help automate the setting needed to reach a desired frequency.

PTM Veröffentlicht am: