Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List Associated Content
Image of Efinix Trion® FPGA and How They Work - Slide16

The Trion® family has multiple means of programming the device. First, there's programming using an external SPI flash device via SPI active mode. The second way, bit banged by a microprocessor or some other device via SPI passive mode, and third, through the traditional JTAG interface. Some of the modes allow wider than x1 configuration, thereby decreasing the configuration time. In SPI active mode, Efinix supports Quad SPI inputs and for the SPI Passive mode, they can support up to x32 bit programming.

PTM Veröffentlicht am: