Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List Associated Content
Image of Efinix Trion® FPGA and How They Work - Slide17

Efinix supports having multiple configuration images in a single SPI flash device. The customer can store up to 4 configurations and then load the one they want. Additionally, Efinix supports a failover to a known good image, the golden image, if there is a configuration error or failed configuration.

PTM Veröffentlicht am: