Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide12

Shown here is a table for the mechanical properties definitions. ASTM standards and procedures are used to determine these mechanical properties. Different TIMs vendors might use different methods/standards of testing. It is always highly recommended for the user to test in the actual application to remove variables that are not taken into account with different standards. In the next few slides, different examples to illustrate the factors or variables impacting mechanical characteristics of Gap Pad. 

PTM Veröffentlicht am: