Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide17

There are other key variables to consider in determining modulus. The boundary conditions take into account other materials friction within the system which might need more stress to compress. As mentioned earlier, the surface area plays a part in the modulus of the material should it be size or shape. The tolerance of the gap in design will affect the amount of pressure exerted onto the material, and the deflection of the material. Another important factor to consider is the time for the relaxation stress on the material. Temperature also affects the factor in pressure when mounting the material to the application. Further discussions in the next few slides will show other variables that affects the stress/strain to the Gap Pad materials.

PTM Veröffentlicht am: